SOC Package Substrate and Application Board Transmission Line Design Engineer
This vacancy has now expired. Please see similar roles below...
Responsible for SoC package substrate and/or application PCB, circuit and artwork
- Define the requirement of SoC package substrate and/or Reference Application PCB
- Specify the outline of the circuit/artwork and define the verification method for it
- Do circuit/artwork design and validate them with the specified method
- Communicate engineers who design circuit and artwork
- Write deltaied technical reports on development outputs
*The full details regarding your position scope as well as any future potential changes in work location and job scope will be provided during the interview process.
- Knowledge of PCB board circuit/artwork design for semiconductor system boards
- Experience with simulation tools to perform signal quality evaluations
- Knowledge of phenomena that affect signal quality, such as transmission loss, reflections, and crosstalk
- Fundamental knowledge about memory devices and interfaces such as DDR, Flash, NVM is plus
- Fundamental knowledge about standards of communication interfaces such as MIPI, PCIe, and else is plus
- Fundamental knowledge in the electrical circuit of digital and analog
SoC products for automotive applications are key parts for realizing the digitization and higher functionality of automobiles, and their evolution is unstoppable. In recent years, higher performance and higher functionality have been realized, and package substrates and application boards are required to meet advanced requirements (e.g., suppression of transmission loss and noise, assurance of signal quality, etc.).
This work involves circuit and artwork design and verification through simulation of signal quality in order to realize PCB boards for package and application systems that meet these requirements. This technology is central to the realization of large-scale systems using chiplets and multi-chip modules, which will improve significantly in the future, and this position will allow the candidate to learn a highly promising technology.
ルネサスは「人々の暮らしを楽(ラク)にする」技術で持続可能な将来を築いていく日本を代表する半導体企業です。自動運転やIoTなど多様な分野において、先進的な製品やソリューションを提供しています。当社の製品は、世界中の主要な電子機器メーカーに採用され、日々の暮らしに欠かせない身の回りのあらゆる電子機器に使用されています。 当社では世界25カ国の製造・開発・販売拠点において20,000人以上の従業員が働いています。グローバルチームとして、すべての従業員が、行動指針である「Renesas Culture」をもとに、互いに学習、協力、成長、目標に向けて前進しながら、日々さまざまな課題解決に取り組んでいます。 当社を取り巻く環境は近年の活発な大型M&Aを含めて、他に類を見ないほどダイナミックに動いています。今後もインフラやデータエコノミー関連の急成長市場でのシェア拡大や、産業/IoTや自動車分野でのプレゼンス強化を図ります。変化の激しい中、グローバルチームの一員として、私たちと一緒に持続可能な将来を築いていただける方をお待ちしています。
VideoUrl
https://www.youtube.com/embed/k-zs4tB6nNc
- Engineering
- Kodaira
- No
Requisition ID
20011063_2024-03-22