IO/PAD Development Engineer for Automotive SoC Design
This vacancy has now expired. Please see similar roles below...
Digital circuit design/verification related to IO, PAD, pin multiplex in automotive SoC (R-Car series)
Target IPs for development: IPs related to IO, PAD, pimultiplex logic
- Specification design of pin multiplex for R-Car SoC IO
- Digital circuit design/verification related to IO, PAD, pin multiplex in automotive SoC (R-Car series), which also includes test pattern design for mass production.
- Management of engineers in Vietnam
*The full details regarding your position scope as well as any future potential changes in work location and job scope will be provided during the interview process.
- Experience of one of IO/PAD/pinmux development in LSI digital front-end design (over 3 years)
- Experience using English in business
There is strong requirement for multi functionality and high performance in automotive SoC, such as "CASE", which make SoC larger and more complex.
As the result, in Renesas, R-Car series is the SoCs which have much bigger and much more functionalities thant other Renesas product.
On the other hand, there is difficulty to make pin multiplex which fulfill customer requirement due to restriction of # of pins and chip size.
Motivated by this, inovative engineers which can deisgn and implemnt pin multiplex specification are recuruited. In addition, generating test program for mass product is also required job.
All customer always uses pixmultiplex so that not only logic design but also customer support are experienceable. Cooperation with design cener in Vietnam requires global mindset.
ルネサスは「人々の暮らしを楽(ラク)にする」技術で持続可能な将来を築いていく日本を代表する半導体企業です。自動運転やIoTなど多様な分野において、先進的な製品やソリューションを提供しています。当社の製品は、世界中の主要な電子機器メーカーに採用され、日々の暮らしに欠かせない身の回りのあらゆる電子機器に使用されています。 当社では世界25カ国の製造・開発・販売拠点において20,000人以上の従業員が働いています。グローバルチームとして、すべての従業員が、行動指針である「Renesas Culture」をもとに、互いに学習、協力、成長、目標に向けて前進しながら、日々さまざまな課題解決に取り組んでいます。 当社を取り巻く環境は近年の活発な大型M&Aを含めて、他に類を見ないほどダイナミックに動いています。今後もインフラやデータエコノミー関連の急成長市場でのシェア拡大や、産業/IoTや自動車分野でのプレゼンス強化を図ります。変化の激しい中、グローバルチームの一員として、私たちと一緒に持続可能な将来を築いていただける方をお待ちしています。
VideoUrl
https://www.youtube.com/embed/k-zs4tB6nNc
- Engineering
- Kodaira
- No
Requisition ID
20011307_2024-03-22