Application Test System Development Engineer for Automotive SoC (R-Car series)
This vacancy has now expired. Please see similar roles below...
Construction of an application test system for automotive SoC (R-Car series)
- Leading the H/W development team for the test board that uses the reference board (control circuit design and artwork design)
- Leading the test S/W development (embedded software development using C, Linux or OS-Less environment)
- Assembling the test system and verifying its operation
*The full details regarding your position scope as well as any future potential changes in work location and job scope will be provided during the interview process.
- Experience of LSI logic design and verification
- Experience of LSI logic synthesis and timing design
- Experience of team management in LSI development
- Experience of LSI evaluation with evaluation board
- Knowledge of software
SoC products for automotive applications are key components for the realization of electronic and advanced functions in automobiles, and their development is unabated. However, as a result of higher performance and functionality than ever before, defects caused by multiple factors that cannot be detected by conventional test methods using ATE (Automated Test Equipment) have become apparent, and the establishment of a system to detect these defects is an urgent task to ensure quality.
This project involves the development of a test board that mimics the SoC application environment and the test software that runs on the board. It also involves the construction of a test system to detect potential defects in the SoC. In developing the board, we will use an existing reference board and guide the engineers responsible for the board circuit design and board artwork design. The test software will be based on existing evaluation software, and the engineers in charge of test software development will lead the development of test software that can run in an OS-less or Linux environment.
This is a very challenging position where you will gain the extensive knowledge required for system integration of leading-edge SoCs.
ルネサスは「人々の暮らしを楽(ラク)にする」技術で持続可能な将来を築いていく日本を代表する半導体企業です。自動運転やIoTなど多様な分野において、先進的な製品やソリューションを提供しています。当社の製品は、世界中の主要な電子機器メーカーに採用され、日々の暮らしに欠かせない身の回りのあらゆる電子機器に使用されています。 当社では世界25カ国の製造・開発・販売拠点において20,000人以上の従業員が働いています。グローバルチームとして、すべての従業員が、行動指針である「Renesas Culture」をもとに、互いに学習、協力、成長、目標に向けて前進しながら、日々さまざまな課題解決に取り組んでいます。 当社を取り巻く環境は近年の活発な大型M&Aを含めて、他に類を見ないほどダイナミックに動いています。今後もインフラやデータエコノミー関連の急成長市場でのシェア拡大や、産業/IoTや自動車分野でのプレゼンス強化を図ります。変化の激しい中、グローバルチームの一員として、私たちと一緒に持続可能な将来を築いていただける方をお待ちしています。
VideoUrl
https://www.youtube.com/embed/k-zs4tB6nNc
- Engineering
- Kodaira
- No
Requisition ID
20011067_2024-03-22