Title:  Sr Staff Application Engineer

Requisition ID:  54120
Department: 
Location: 

Seoul, GANGNAM-GU, KR

Job Function:  Applications Engineer

Sr. Staff Application Engineer

 

Description:

Seeking an experienced Application engineer to work with the Renesas Memory Interface Validation and Apps team on state-of-the-art products such as RCD and data buffers.  This is a position with high visibility and high growth potential.

 

Duties/Responsibilities

  • Support product development life cycle from conception to production release. This involves interfacing with multiple functional teams including Design Engineering, Test Engineering, Quality Assurance, and other engineering groups.
  • Achieve thorough and methodic understanding of requirements and challenges from the application environment.
  • Continuously expand detailed knowledge of Renesas Memory Interface product offerings.
  • Work with customers to help them achieve their goals and solve problems.
  • Write application notes and other documentation for external customers and partners, as well as for internal company users.
  • Develop solutions to help maximize performance of Renesas products in the user application environment.
  • Participate in the development of new product specifications to help ensure Renesas products will remain competitive in the field.
  • Design and debug hardware and software for lab validation and qualification purposes.

 

Preferred Skills/Knowledge 

  • 8+ years of direct experience in post-Silicon applications, debug, and validation.
  • Strong knowledge of DDR3/DDR4/DDR5 and/or SERDES protocols, testing and application.
  • Familiar with computer system architecture, especially for Intel x86 server system.
  • Skilled in the use of lab equipment such as oscilloscopes, pattern generators, ATE, Logic Analyzers.
  • Skilled in test automation development using Python.
  • Experience in high-speed test board design, analysis, and debug.
  • Familiarity with DIMM RCD, Data Buffer and I2C and I3C devices is a plus.
  • Good writing skills desired.

 

Education

  • Master’s Degree in Electrical Engineering, Computer Engineering, or related, with 8+ years of relevant experience.
  • Bachelor's Degree in Electrical Engineering, Computer Engineering, or related, with 12+ years of relevant experience.